Puerto Rico - Marcar Puerto Rico

Confirme su elección de moneda:

Bench Talk for Design Engineers

Bench Talk

rss

Bench Talk for Design Engineers | The Official Blog of Mouser Electronics


AS6496 Anti-Counterfeit Control Plan Posted Chuck Amsden

The AS6496 standard was published in August and Mouser now has an Anti-Counterfeit Control Plan written specifically to that standard.

In addition to the clauses of AS6496, Mouser has incorporated additional requirements in the plan that address DFARS 252.246-7007.

AS6496 meets the intent and fulfills the requirements of the 9 of 12 points. The additional points are: 10 Process for keeping continually informed of current counterfeiting information and trends; 11 Process for screening GIDEP reports; and 12 Control of obsolete electronic parts. These additional requirements are covered by our Anti-Counterfeit Control Plan posted on our website. Visit https://www.mouser.com/pdfdocs/QS-PR-024.pdf



« Back


Chuck AmsdenChuck Amsden is the former Vice President of Quality at Mouser Electronics. Amsden joined Mouser in 2003 and helped lead the company to obtain ANS9120A/ISO9001:2008 and ANSI/ESD S20.202007 certifications. Amsden was a contributing member of three SAE G-19 committees, working on standards for mitigating counterfeits in the electronic components supply chain. He also chaired a committee in the Electronic Components Industry Association (ECIA) that developed methods of traceability within authorized distribution and served on the ECIA Certification Task Force focused on mitigating counterfeits.


All Authors

Mostrar más Mostrar más
Ver mensajes por fecha

Archivos