Puerto Rico - Marcar Puerto Rico

Confirme su elección de moneda:

Bench Talk for Design Engineers

Bench Talk

rss

Bench Talk for Design Engineers | The Official Blog of Mouser Electronics


New Tech Tuesdays: USB 3.2 Gen 2x1: High-Speed Design Made Simple Mouser Technical Content Staff

New Tech Tuesdays

Join Mouser's Technical Content team for a weekly look at all things interesting, new, and noteworthy for design engineers.

USB Type-C is everywhere, from smartphones to industrial control panels, and with it comes a long list of USB standards. While USB4 and USB 3.2 Gen 2x2 offer sufficient bandwidth to grab headlines, not every design calls for the complexity that comes with those higher speeds. For many embedded applications, USB 3.2 Gen 2x1 is a practical sweet spot, offering 10Gbps over a single lane, with lower power and simpler routing requirements.[1]

USB 3.2 Gen 2x1 is fast enough for high-resolution imaging, sensor data acquisition, and portable diagnostic tools, while avoiding the tight design tolerances and dual-lane layout headaches of higher-tier protocols.[2] For engineers working on FPGA platforms, edge artificial intelligence (AI) systems, or test equipment, Gen 2x1 offers an ideal solution.

What Makes USB 3.2 G 2x1 a Smart Design Choice?

USB 3.2 Gen 2x1 offers 10Gbps transfer speeds using one lane over a USB Type-C connector, which is twice the bandwidth of USB 3.2 Gen 1x1 while remaining fully backward-compatible with earlier standards. But the benefits go beyond the numbers on a spec sheet.

Unlike Gen 2x2 or USB4, which rely on dual-lane routing for peak throughput, Gen 2x1 transfers all data through a single high-speed differential pair. This simplifies PCB layout, especially in space-constrained environments or where signal integrity is important.[3]

Engineers also avoid many of the complications that come with faster multi-lane USB designs. USB 3.2 Gen 2x1 can:

  • Reduce the chances of signal interference between traces
  • Ease timing constraints that can cause errors
  • Lower power consumption, reducing thermal load
  • Exhibit less EMI, improving compliance in sensitive environments

For systems that do not require full 20Gbps to 40Gbps transfer speeds, Gen 2x1 offers enough headroom to handle real-time video, high-speed data logging, and other bandwidth-intensive tasks, without requiring high-end layout tools or costly re-spins.

What Dual-Lane USB Adds—And Why You May Not Need It

USB 3.2 Gen 2x2 and USB4 leverage two lanes to achieve 20Gbps and beyond, but that bandwidth comes with design tradeoffs. Dual-lane routing doubles the trace count, increases routing density, and introduces greater sensitivity to impedance mismatches, jitter, and reflections.

At these speeds, PCB stack-up, via stubs, connector quality, and even trace length matching can create problems that are easier to manage in single-lane Gen 2x1 designs. These challenges are more pronounced in dual-lane designs, such as Gen 2x2, where timing and integrity must be maintained across multiple lanes. On the other hand, Gen 2x1’s single-lane setup is simpler to route and often avoids the need for advanced signal conditioning, like equalization or de-emphasis.

Unless your application truly requires top-tier throughput (e.g., external GPUs, raw 8K video pipelines, multi-channel data streaming), these additional design demands may not justify the upgrade. Gen 2x1 offers a cleaner, more accessible path to high-speed USB.

The Newest Products for Your Newest Designs®

For engineers developing USB 3.2 Gen 2x1 applications, a key challenge is testing high-speed data paths in real hardware, especially when integrating with FPGA platforms. This week’s New Tech Tuesdays featured product is the Infineon Technologies EZ-USB™ FX10 Development Kit (DVK), which helps in this matter.

This compact kit features an FPGA Mezzanine Card (FMC) interface, making it easy to connect the FX10 controller to most standard FPGA development boards. Engineers can prototype USB Type-C–based designs with minimal setup, making it ideal for applications such as video streaming, data acquisition, and embedded diagnostics.

Example use cases include machine vision systems, 3D scanners, and video frame grabbers, where high-speed USB performance is required with minimal latency.

Tuesday’s Takeaway

As USB standards evolve, USB Type-C is poised to support even faster data rates, higher power delivery, and alternate modes like DisplayPort and Thunderbolt. But with increasing complexity, Gen 2x1 remains a solid choice for many systems.

USB 3.2 Gen 2x1 is already compatible with USB Power Delivery (USB PD), enabling negotiation of voltages and currents up to 100W in many designs. It also supports Alt Modes, allowing devices to share the USB Type-C connector for video output or other functions without needing the full USB4 stack.

USB 3.2 Gen 2x1 offers the right combination of performance and simplicity for modern designs. It lets engineers build high-speed USB Type-C–based devices that are reliable, scalable, and easy to manufacture.

   

[1] https://www.usb.org/usb-32-0
[2] https://www.ti.com/lit/an/scaa144/scaa144.pdf
[3] https://www.kingston.com/en/blog/personal-storage/usb-3-2-gen2x2



« Back


Mouser Electronics, founded in 1964, is a globally authorized distributor of semiconductors and electronic components for over 1,200 industry-leading manufacturer brands. We specialize in the rapid introduction of the newest products and technologies targeting the design engineer and buyer communities. Mouser has 28 offices located around the globe. We conduct business in 23 different languages and 34 currencies. Our global distribution center is equipped with state-of-the-art wireless warehouse management systems that enable us to process orders 24/7, and deliver nearly perfect pick-and-ship operations.


All Authors

Mostrar más Mostrar más
Ver mensajes por fecha

Archivos