Mouser Now Stocking Maxim's MAX22195 High-Speed Octal Digital Input for PLC and Automation
February 14, 2019 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the MAX22195 octal industrial digital input device from Maxim Integrated. Designed to reduce power, system cost, and size for programmable logic controller (PLC) digital-input subsystems, the MAX22195 is a highly integrated IEC 61131-2-compliant digital input device for industrial, process, and building automation applications.
The Maxim MAX22195, available from Mouser Electronics, translates eight 24 V industrial inputs to a serialized CMOS-compatible, parallel outputs with propagation delay of less than 300 ns from input-to-output for all channels. The fault-tolerant, 5 mm × 5 mm device interfaces with 3 V or 5.5 V logic and incorporates a current-setting resistor, allowing engineers to configure the MAX22195 for IEC 61131-2 Type 1, 2, or 3 inputs. The MAX22195 includes an internal low dropout (LDO) regulator that provides power to digital isolators and other field-side circuits, plus energy-less field-side LED drivers that meet the indicator light requirement of IEC 61131-2 with no additional power dissipation.
The MAX22195 also offers surge protection to ±1 kV and ±8 kV contact electrostatic discharge (ESD) and ±15 kV air gap ESD protection to contribute to increased system robustness. The MAX22195 device is supported by the MAX22195EVKIT evaluation system, which provides terminal blocks for all eight inputs and a single header for all eight outputs for easy monitoring and evaluation. Eight field-side LEDs indicate input status, and a READY LED indicates that the MAX22195 is operating normally.
To learn more, visit www.mouser.com/maxim-max22195-interface.
With its broad product line and unsurpassed customer service, Mouser strives to empower innovation among design engineers and buyers by delivering advanced technologies. Mouser stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is continually updated and offers advanced search methods to help customers quickly locate inventory. Mouser.com also houses data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.
About Mouser
Mouser Electronics, a Berkshire Hathaway company, is an award-winning, authorized semiconductor and electronic component distributor focused on rapid New Product Introductions from its manufacturing partners for electronic design engineers and buyers. The global distributor's website, Mouser.com, is available in multiple languages and currencies and features more than 5 million products from over 750 manufacturers. Mouser offers 23 support locations around the world to provide best-in-class customer service and ships globally to over 600,000 customers in more than 220 countries/territories from its 750,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.
About Maxim Integrated
Maxim is the leader in analog integration. From mobile to industrial solutions, Maxim is making analog smaller, smarter and more energy efficient.
Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
(817) 804-3833
Kevin.Hess@mouser.com
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com